Part Number: DS560DF410
Other Parts Discussed in Thread: DS560DF810
We are using the DS560DF410 device on a custom board. We are using it to communicate with a processor via SFP+ interfaces (ethernet interface), and everything works correctly when we use an FTDI to initialize the device using your API via IIC. The device functions properly with the default parameters. We only needed to enable the channels on the two DS560DF410s.
We have included an EEPROM for each device on the PCB and would like to program them for production units. However, we cannot find a default project with the EEPROM memory content. Could you kindly provide us with the default configuration for initializing the device with its default settings? We only need to activate the four channels on the DS560DF410.
Regards and thank you very much.