This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90C3202 Temperature Capacity

Hi all

There are the following questions in "Absolute Maximum Ratings" table of DS90C3202 data sheet.
1. "Package Derating" What is meant?
2. Although theta(ja) is not indicated, what value is it?
3. Although written as "Maximum Package Power Dissipation Capacity at 25C"=1.4W,
   Worse Case(max) of "Figure 6." =550mA and it is set to 3.3Vx0.55A=1.815W,
   Isn't "Maximum Package Power Dissipation Capacity" exceeded?

best regards

Hisa Kobayashi