This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM3730+TUSB1210

Other Parts Discussed in Thread: TPS65920, DM3730, TUSB1210

HI

   

We have problems in debugging arm USB communication at present, when the device is powered up or reset, the link is not  find the lna9513.

We use the following:

     DM3730.usb0  connect to  TPS65920   apply in OTG;  open this link

     DM3730.usb1  connect to  TUSB1210   apply in Host  link to LNA9513 USB hub.

We use the Tusb1210  ULPI input-clock mode 

2063.dm3730 usb.doc

But 

    We canot  find the device on the USB1;  the ULPI  CLK as bellow:

And  we should see the signal on the dp/dm as bellow:

  • Problem Description:

    We are using the USB port of DM3730 encountered the following probl6888.问题描述.docems:

    ARM itself only recognizes the three USB HOST port, failed to identify the peripheral USB HUB, the application used the TI DM3730 + TPS65920 + TUSB1210.

    ARM's USB port usage is as follows:

    OTG mode: DM3730.USB0 connection tps65920, which is reserved for the usb port;

    HOST mode: DM3730.USB1 connection TUSB1210 USB phy, connecting peripherals USB HUB LAN9513;

    By USB1 port TUSB1210 phy LAN9513 not recognize peripherals connected to, but the peripherals LAN9513 jumper to tps65920 reserved interfaces, able to identify to the peripheral HUB.

    Therefore, whether to apply TUSB1210 where there is a problem?

    TUSB1210 use the ULPI interface (input clock mode) ,SCH as bellow:  in the file

    REFCLK tied low to GND,ID tied low to GND,CS,RESET tied high to vcc1V8,VBUS supply external

     5V,VDD3V3  Connect to external filtering capacitor.

     measuring the ULPI inferface clk ,as bellow:60Mhz    in the file

    We can measure the ware on the DP/DM of TUSB1210,as bellow: in the file

    Have  three  question :

        1.What is cause of the square ware about 800Khz;

          2.what way to decide  the TUSB1210 is really work with average;

          3.what problem with this applition?

  • Hello abc,

       We are reviewing Your post and We will reply soon.

    Regards,

    Diego.