This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Our customer has a question about the quad RS422 driver & reciever : AM26C31&AM26C32.
I'm posting the question for a customer:
++++++++++++++++++++++++++++++++++++++++++++++
When some drivers and receivers are not used ,
what to do with unused pins ?
(pull-up, pull-down or floating?)
AM26C31: input:A , output:Y/Z
AM26C32: input:A/B , output:Y
++++++++++++++++++++++++++++++++++++++++++++++
thanks in advance.
Takishin-san,
The RS422 lines A,B,Y,Z do not need any connection, floating is good.
The digital outputs can float too.
The digital inputs must be terminated to ground or VCC. A series resistor is recommended (1k to 100k), but not required.
AM26C31 input A,G,and ~G should be terminated to VCC or GND. Y and Z can float.
AM26C32 input G,~G should be terminated to VCC or GND. A, B and Y can float.