This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Conf. DP83630-EVK to perform PPS

Other Parts Discussed in Thread: DP83630-EVK

I'm am trying to configure DP83630-EVK to output Pulse Per Second (PPS) on one of the GPIO ports.
I am using an FPGA based embedded system and greatly reduced EPL C library to configure the DP83630-EVK.
I use the following configuration, from Software Design Guide and C Software Reference Library:

    PTPEnable( pEPL_HANDLE, FALSE);
    PTPClockSetRateAdjustment( pEPL_HANDLE, 0, FALSE, FALSE);                   //dolje
    PTPClockSet( pEPL_HANDLE, 1, 0);
    PTPSetClockConfig( pEPL_HANDLE, CLKOPT_CLK_OUT_EN, 0x0A, 0x00, 8);
    PTPEnable( pEPL_HANDLE, TRUE);
                                                                                //gore
    // Configure Trigger 0 for PPS – only perform if using PPS
    PTPEnable( pEPL_HANDLE, FALSE);
    PTPSetTriggerConfig ( pEPL_HANDLE, 0, TRGOPT_PERIODIC|TRGOPT_NOTIFY_EN, 9);
    PTPArmTrigger( pEPL_HANDLE, 0, 10, 0, FALSE, FALSE, 500000, 0);

After this I expect to see a PPS at GPIO9 but it doesn't happen. Only change is a pulse that appears at CLK_OUT pin (pictures bellow).

Questions:

Am I wrong to expect PPS output after this configuration?
Is GPIO9 available for output?

Additional information:

DP83630-EVK jumpers used:
J12 - USB_3v3         J33 - auto-negotiation
J3   - PMDIO_MII       J36
J4   - PMDC_MII         J39

Reg_val after configuration:
PHY_PG5_PTP_TRIG: 0x5900