This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD23 Output Failure

Other Parts Discussed in Thread: SN65HVD23

I have a customer who is using the SN65HVD23 between a Control PC and a radar transmitter. The device output is failing to the PC and in a permanent low state when failure occurs.

Customer called to report that the chip is burning out 1 every 40 hours. The customer believes something external on the load side may have lead to its destruction. My question pertains to the likely cause of these failures… The customer expecting a load transient, but wanted to be sure that the chip is protected from an over-current output condition (which was communicated to the customer) and would like to know how long the device can handle an over-voltage event and how high a voltage before damaging the device.

  • The maximum voltage before damaging the device is specified in the data sheet under Maximum Ratings.

    How long an overvoltage can be tolerated depends on the transient energy (voltage, current, and time). The specified 16kV ESD HBM only consider relative low current for a few nano-seconds. Higher energetic transients require external transient-voltage-suppressors (TVS) such as PSM712.

    Please see attached application report.

    Best regards,

    Thomas

     

     

     

    RS-485 Transient Protection.pdf