Hello,
The data sheet for the TSB81BA3D indicates a VOD output level for TPA and TPB of 265mV max into 56 ohms.
I actually measure a VOD on both TPA and TPB of about 740mV pk-pk when I have an active 1394B S800 connection between two TSB81BA3D ports. I am working on a design where I want to interface the TPB pins to an optical transceiver whose minimum differential voltage requirement is 400mV.
Based on my measurements, I should be ok, but based on the repeater data sheet I would probably want to use a (SN65CML100) buffer to the optical part.
Can you please advise me on the VOD output levels?
Thanks,
Mitch
I have a design for a 1394B optical repeater using the TSB8BA3D with the TPB +/- pins terminated as shown in the data sheet driving the Tx pins of the AC coupled 100 ohm terminated optical transceiver.