This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I just received an ISO5500EVM. I was planning to populate an IGBT and use it to switch up to 600VDC. It looks like there isn't enough clearance between the source and drain traces to support this voltage. The source is connected to the plane on the bottom of the board and there are many vias, including some in the drain tracks that have small (less than 10mil) annular rings.
Has anyone used this eval module with a significant voltage? If so, how high?