This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Different voltage on last bit CAN message SN65HVDA1050A-Q1

Hello,


when viewing the CAN messages on our product (J1939 protocol) we discover that the last bit has a different voltage:

design:

CAN_Tx, CAN_Rx : to Piccolo DSP

CAN_High_inp, CAN_Low_inp : to connector of the product

setup:

product connected to USB/CAN device from National Instruments (ref: USB-8473) with 1m cable and 120 Ohms resistor close to USB/CAN device

we have different products using the same CAN interface design and this phenomenon is obervable on all products.
Do you have an explanation for that? could it be critical?

thanks in advance for your reply,

Benoit