I have a question regarding Texas Instruments DS90LV028AH High Temperature 3V LVDS Dual Differential Line Receiver. A 100 ohm input termination resistor is recommended in the specification. What are the effects if a termination resistor is not used? The receiver detects an input representing a Built in Test function that is either in the ON condition or the OFF condition. If a termination resistor is not used, will there be erroneous switching due to noise or other factors?