This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB211 - not activating

Other Parts Discussed in Thread: TUSB211, USB-REDRIVER-EVM

Hi,

I developped a small board which interface a TUSB211, two USB connectors and a voltage regulator to convert one side's VBUS to the TUSB211 necessary 3V3 power supply (see attached schematic).

I'm doing some eye diagrams with an appropriate Agilent scope and a host generating test packets.

The TUSB211 has no effect; I compared with a board without the TUSB211 and it does not change a thing.

I also tried with various value of EQ resistor, still no effect.

ENA_HS and CD are always at 0V, so is VREG.

Toggling the RST pin also has no effect.

Any help would me very appreciated.