This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help with selecting FPD-Link III combinations with coaxial connection



I would like to have a single FPD-Link receiver with two interchangeable input serialisers: a 720p HDMI input and a 720p Bayer/YUV input. The receiver needs to output either Bayer or YUV. The connection needs to be coaxial.

Assumption: DS90UB914A is the only deserialiser I found capable of Bayer/YUV output with a coaxial connection. That would be fine on it's own, but I cannot connect a HDMI serialiser directly to it, can I? Every HDMI serialiser I checked didn't have DS90UB914A listed as a possible receiver IC.

Are there other deserialiser with coaxial input that can be used to output Bayer/YUV having compatibility with both a Bayer/YUV and HDMI serialiser?

Thank you.