Hello,
We're using a DS34C87T driver in our product and one of our customer ask if he can use it with a consecutive electronic which requires a differential voltage min of 2.5V.
Regarding the spec of the product below, the minimal differential voltage for the driver is 2.0V with the specified supply of 5V +/-10% = 4.5 to 5.5V.
Question: if customer monitor the voltage supply and guarantee that this will not drop under 5.0V, can we certify that output differential voltage would be 2.0 + 0.5V = 2.5V ?
Or what parameter could help to increase this voltage ? Driver load would be approx 100 Ohm.
Thanks for help.