This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI TUSB2077A

Other Parts Discussed in Thread: TUSB2077A

I have implemented a self-powered USB hub using the above device.  When I connect the upstream port to a PC, the PC recognizes the hub.  When I plug a device (e.g., thumb drive) int a down stream port, the PC sees it and the files.  I can access the files on the thumb drive.  However, when I connect the upstream port to the PC ALL downstream ports are powered up within about 0.5 seconds, regardless of whether or not there is ANY USB device plugged into any port (i.e., even when no device is plugged into a down stream port>) It seems that the PC is telling all ports to power up.  I want the hub to apply power only to the ports that have a USB device plugged in (as do most hubs).  What must be done to make this so?

Leland