This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps65982 pp_ext wait for SRDY quetsion



Hi

In 65982d, I set 0x28 bit30~28 to be 011 in firmware, it mean the power cannot enter system without SRDY command via PP_EXT.

When 982d power on from dead battery mode, the power can enter to system via PP_EXT.

However, there is no way to turn off besides disable pp_ext in 0x28.

But in 982 v1.11.05 firmware and same condition, i can turn off the power path by SRYR.

Can i know which behavior is correct and my customer ask this function in some use case.

BTW, in 0x1a, 982d show pp_ext is disable and 982 show it is sink power from above case.