Part Number: TPS65982
Hi Team,
My customer would like to know how long it will take for TPS65982 to receive the HPD signal and output it with the CC command in UFP use case.
Do you have any data on the delay?
Regards,
Takashi Onawa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS65982
Hi Team,
My customer would like to know how long it will take for TPS65982 to receive the HPD signal and output it with the CC command in UFP use case.
Do you have any data on the delay?
Regards,
Takashi Onawa
Hi Onawa-san,
The total delay for the TPS65982 to receive the HPD signal includes both HW delay and FW delay. The two states where HPD occurs is from High to Low(unplug) and Low to High(plugged).
Total for High to Low = 1.617ms
Total for Low to High = 0.577ms
Regards,
Jimmy Hua
Consider checking the "Verify Answer" button if I've answered the question to your satisfaction.
Hi Onawa-san,
To be more specific, the HPD have a HW and FW latency. Below is a breakdown of the two type of delays:
A. HW state machine delay + interrupt latency (time from HPD change until FW enters interrupt service routine)
B. FW latency (time from interrupt service routine start to PD message starts)
“A” can change based on different HW state machine delays which can be calculated.
“B” seems to be fixed at 217 us for a typical case.
For High to low transition I see A=1.4 ms
For Low to High transition I see A= 0.36 ms
Total for High to Low 1.617 ms
Total for Low to High 0.577 ms
To answer your question:
1. The time calculated can be variable depending on the HW delays. The FW delay seems to be consistent at 217us(typical).
2. Those time values are for typical use cases.
Regards,
Jimmy Hua