Part Number: TPS65982
Dear,
My question is related to the TPS65982DC, and here are two questions want to ask:
1. In the FW setting, If the sleep mode is enabled, when the system will enter into sleep and when it will out of the sleep mode?
2. For the HPD for DP, I set GPIO4 as the HPD function, when there is no DP device, the GPIO4 output will be float or set low? and is it when DP device inserted, the HPD will set high, am I right?
Thanks.