Part Number: DS91C176
Hi Team,
The customer is using DS91C176. The customer uses 100ohm as the matching resistance. But the signal is not fine. Please check the attach.
The Figure 19 of the datasheet shows the relationship between the VOD and the output load.
Q1: I would like to know what the VOD is. Is it the differential voltage between A pin and B pin or the differential voltage between R pin and RE pin?
Q2: In the figure 1 of the datasheet, the matching resistance is 80 ohm on the ATCA backplane.
How to select the matching resistance?
Can I refer to the figure 19 of the datasheet to select the matching resistance, for example, if the VOD is 500mV, then the matching is needed 40ohm?
Q3: How to improve the signal quality for DS91C176?
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments