Part Number: DS90UB929-Q1EVM
Other Parts Discussed in Thread: USB2ANY
Hi,
I am using Analog Launch Pad GUI to interface to my DS90UB929 (serializer) --> DS90UB926 (deserializer) boards. I am having trouble detecting the first board on the GUI. After I select the right board from the USB2ANY profile list, I see the correct board with I2C address and board number but I cannot get the HDMI communication to confirm on the GUI.
All the settings are default and Hot Plug has been asserted. When I probe the SMA connectors on the output I see bits flipping and data being sent irregardless of having an HDMI input or not. My eye chart looks really good, but I cannot confirm if the HDMI is being sent through, because I see the same thing even when I remove my HDMI cable. Can someone help me confirm if my 929 serializer is working correctly?