Other Parts Discussed in Thread: SN74LVC1G57
I am using DS26LS31C for driving high speed optocoupler which is on different board. Max cable length is 10ft and I have used twisted pair shielded cable. Max transfer rate required 1Mbit/sec. Environment is very noisy and hence looking for driver IC which has 3.3/5 volt input and differential output with 12/24 Volt DC signal.
Pl suggest suitable alternative which can handle 12 or 24 Volt DC differential signal.