Part Number: SN65HVD1176
We are looking for a bus solution for up to 300 nodes were the nodes are mounted relatively close to each other (spacing 5cm).
While reading the 'Device spacing on RS-485 buses' Analog Applications Journal (http://www.ti.com/lit/an/slyt241/slyt241.pdf I noticed that there is a minimum node spacing when using a RS-485 driver.
The document is referring to the SN65HVD1176, which is a half-duplex driver.
I would like to know if this minimum node spacing is only applicable for half-duplex drivers or also for full-duplex RS-485 drivers?