Part Number: TCA9548A
Hi experts,
I got some questions from customer on TCA9548A. Could you please kindly comment on them? Thanks!
1. Could you explain in more detail (or give examples) on the terminology “tpd” and “trst”?
2. For “trst”, from note (2) in above, it means “the propagation delay measured from the time the RESET pin is first asserted low to the time the SDA pin is asserted high”. Could you identify “trst” in below picture?
Note: Yellow is RST, violet is SCL, and green is SDA.
3. For “trst”, it is 500ns maximum, while, in note (2), “It must be a minimum of tWL.” Does that mean tWL< trst <500ns ??
4. For “tpd”, what does “from SDA or SCL(INPUT) to SDn or SLn(OUTPUT)” mean? For instance, does it mean the time from the falling SCL to the rising SDA in a read operation? Like the red cycle marked in below picture?