Part Number: TUSB1002EVM
Other Parts Discussed in Thread: TUSB1002,
Hello, my setup is:
Host PC ------>(USB A to USB B cable 0.5 m)--------->TUSB1002EVMRe-driver------------> USB 3.0 stick memory
Host PC ------>(USB A to USB B cable 0.5 m)--------->TUSB1002EVMRe-driver------------> (USB A to USB A cable 1.5 m)-------------------> USB 3.0 stick memory
I've tried USB 3.0 and 3.1 ports,
I've also tried different jumpers configuration for the EQ and Config
But the behavior is always the same: I see the device behind the Re-driver in USB 2.0 mode.
I cant get transfer rates over 40 MB/s
Note that with USB 3.0 windows advises that the device can be connected to SS port.( it is already connected to SS port)
I've tried also in linux and I could check that the connection detected was 2.10 same as windows.
So I'm out of ideas to figure out how to see a device behind this re-driver working successfully at 3.0 Mode.
Thanks in advance for the answers.