This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Input protection for SN65HVS883

Other Parts Discussed in Thread: SN65HVS883

I am using SN65HVS883 to detect the digital input signal for industrial . I had seen the datasheet and found that it has ESD protection and require a MELF resistor and capacitor. Normally, My input signal is 10 to 30 V and field supply voltage is 12V. My question are following:

1. Do I need more external protection for input such as overvoltage, surge protection?

2. Can I apply the input voltage more than field supply voltage?

3. If I don't want to place the LED at REx pin. How can I do to this pin?