This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65986: TPS65986 Short Circuit reliability

Part Number: TPS65986

I have an application where it is likely that the USB Type C cable can become sheared to the point where VBUS gets shorted to GND through the cable. In my system VBUS is 5V. I have two TPS65986EVMs connected with a proper type C cable and I am testing shorting VBUS to GND. When I do this, the DFP TPS65986 goes into a state where the internal power switch opens and does not close again until I assert the HRESET signal.The desired behavior is that once the short condition is removed the TPS65986 will attempt to close the switch again. How do I get the TPS65986 to auto retry closing the power switch? Is this a particular firmware setting or am I forced to use an external circuit to trigger the HRESET signal?

Thanks,