This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: Review of the schematic required for current design

Part Number: DP83867IS


Need someone from TI to verify current design with DP83867IS ethernet PHY with T4080 processor from NXP. Using a built in magnetic port as in schematic. Need to check that if it is compatible and any other item which seems incompatible. Also the IOs are set to 1.8V through processor. To check if voltage translation is required.