Part Number: TCA6424A
Hi all
Would you mind if we ask TCA6424A?
<Question1>
After /Reset asserted, all ports will return to initial condition.
So, the default setting of all ports are input, right?
<Question2>
In relation to <Question1>, when the port setting is input(default setting), if we sent output command(Output Port Registers) without configuration setting,
-Will the device operate with input? Or output command will be destroyed??
-In this case, will ACK command output from the device normally?
Kind regards,
Hirotaka Matsumoto