Other Parts Discussed in Thread: SN65LVDS180
This parameter ICC is stated 4 ways on the datasheet, once for active and 3 ways for disabled conditions. I am having trouble meeting the 1mA limit at -40C for the "Disabled" test.
There are no setup conditions given but I assume the DE pin is driven low and /RE pin drive high. I am using 0V and VCC on those pins and believe all other inputs are don't care. VCC is 3.6V during the test. The test works fine at room and hot but fails many of my samples at cold. I am hoping to get some insight into the manufacturer's test setup conditions, and make sure this is actually production tested. Also it might be helpful to know what is the difference between SN65LVDS180-Q1 and SN65LVDS180?