Hi~
Does TPD1E05U06 has polarity?
Customer used this part but some of the circuit level was clamped to 0.8V(0V - 0.8V logic level). When remove diode on this line, line was normal up to 3.3V level.(0 - 3.3V level)
I wonder if it has polarity, like pine 1 should connect to signal and 2 should be gnd, or, etc....
And how can I test if it is right or not.
Thanks