This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to configure the device in sleep mode so that any switch state change it gives interrupt to MCU
and for interrupt mode, the trigger is required or not. what is the proccess for it
DEVICE_ID = 0x01000000;
INT_START = 0x02000000;
CRC = 0x0300FFFF;
IN_STAT_MISC = 0x04000000;
IN_STAT_COMP = 0x05000000;
IN_STAT_ADC0 = 0x06000000;
IN_STAT_ADC1 = 0x07000000;
IN_STAT_MATRIX0 = 0x08000000;
IN_STAT_MATRIX1 = 0x09000000;
ANA_STAT0 = 0x0A000000;
ANA_STAT1 = 0x0B000000;
ANA_STAT2 = 0x0C000000;
ANA_STAT3 = 0x0D000000;
ANA_STAT4 = 0x0E000000;
ANA_STAT5 = 0x0F000000;
ANA_STAT6 = 0x10000000;
ANA_STAT7 = 0x11000000;
ANA_STAT8 = 0x12000000;
ANA_STAT9 = 0x13000000;
ANA_STAT10 = 0x14000000;
ANA_STAT11 = 0x15000000;
ANA_STAT12 = 0x16000000;
CONFIG = 0x1A00040C | 0x00001000 | 0x00000800;
IN_EN = 0x1BFFFFFF;
CS_SELECT = 0x1C0003FF;
WC_CFG0 = 0x1DB6DB6D;
WC_CFG1 = 0x1E16DB6D;
CCP_CFG0 = 0x1F000000;
CCP_CFG1 = 0x20000000;
THRES_COMP = 0x21000000;
INT_EN_COMP1 = 0x22FFFFFF;
INT_EN_COMP2 = 0x23FFFFFF;
INT_EN_CFG_0 = 0x24000004;
INT_EN_CFG_1 = 0x25000000;
INT_EN_CFG_2 = 0x26000000;
INT_EN_CFG_3 = 0x27000000;
INT_EN_CFG_4 = 0x28000000;
THRES_CFG0 = 0x29000000;
THRES_CFG1 = 0x2A016800;
THRES_CFG2 = 0x2B00D247;
THRES_CFG3 = 0x2C045C77;
THRES_CFG4 = 0x2D0CBDA2;
THRESMAP_CFG0 = 0x2E000000;
THRESMAP_CFG1 = 0x2F023000;
THRESMAP_CFG2 = 0x300001F5;
MATRIX = 0x31000000;
MODE = 0x32000000;