This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1043HG-Q1: Vsup Pin in TCAN1043HG- Q1

Part Number: TCAN1043HG-Q1
Other Parts Discussed in Thread: TCAN1043, TCAN1043H-Q1

Hello Sir,


I am looking into Automotive CAN transceivers for our application, I came across TCAN1043HG-Q1, I am not sure why the Vsup is used for. 




Thanks 

Akilan G 

  • Akilan,

    VSUP is meant to be the connection to car battery, it supplies the internal LDO that is the reference for the digital logic. The other two power inputs, VCC and VIO supply the CAN bus and the TXD and RXD levels, respectively.

    Please let me know if you have any other questions.

    Regards,
  • Hey Eric, Thanks for quick reply.

    Okay. So, can the Vsup and Vio be an optional if necessary. Because I see in reference design, the Vsup is directly grounded.


    And Also, Could you tell me about INH pin.


    Akilan G
  • Akilan,

    No, VSUP is not optional. Can you refer me to the reference design where VSUP is grounded?

    INH is an output that is pulled up to VSUP and is meant to be used to supply another power supply on board (LDO or SMPS). It is disabled in Sleep mode, and enabled in Standby and Normal modes. The intent for the output is to supply an on board power supply IC that will provide power to the MCU controlling the TCAN1043. In sleep mode, which is a low power consumption mode, the INH pin is low, so the on board power supply is off, and thus the MCU is off. The TCAN1043 will then receive a wake up request through the bus and go into Standby mode. In Standby mode, the INH supply will come back up, and supply the LDO or SMPS providing power to the MCU, which will send a signal to the EN pin on the TCAN1043, and the device will be in Normal mode.

    This isn't the only way to use the pin, but this is the typical and intended use in most low power applications. I made a lot of assumptions about your understanding of the device in that explanation, so if there is something you didn't quite understand, let me know and I will elaborate.

    Regards,
  • Hey Eric,


    The explanation is very helpful. I understand the INH Pin now.

    I am attaching the png file of the circuit where the VSUP is grounded.




    Akilan G 

  • Akilan,

    The schematic shows the VSUP net name on the pin with the decoupling capacitor, C5. If you look at the entire schematic, VSUP is most likely somewhere else, and that net name is referencing that point in the circuit, so you don't have to show the physical connection in the schematic and have wires crossing over each other unnecessarily.

    Let me know if that makes sense.

    Regards,
  • Makes sense. So, I can give 70 V on VSUP. Right ?
  • If you have the TCAN1043H-Q1 or the TCAN1043HG-Q1 versions of the device, yes, you can. But there will be little to no margin for any extended voltage spike. Will there be 70V on VSUP in the application?

    Regards,
  • Got it. No, In our application its 48 volts. And your answers are really helped.

    Thank you,
    Akilan G
  • Akilan,

    Great, glad to help! Is there any way you can click 'Resolved' on my posts? It helps with managing the E2E forums.

    Regards,
  • Sure, Thanks again Eric.



    Regards,
    Akilan G