Part Number: TPS2553D
Other Parts Discussed in Thread: TPS2553, LM5005
Hello Team
My customer is using the TPS2553 as a load switch in the circuit below with overcurrent set to nominal 266mA. They are testing their boards and found on some boards, the FAULT flag in not active even though the part is in current limit with output voltage collapsing as internal FET is in linear region. They are using resistive load and gradually dropping the resistance while monitoring the output voltage and FAULT flag. The FAULT flag only goes active when the output has collapsed <1V.
Vin = 5V
Load Vout Fault
15 Ohm 3.7V High
13.5 Ohm 3.55 High
10 Ohm 3 High
8.2 Ohm 2.8 High
6.8Ohm 2.55 High
5.1Ohm 2.4 High
3 Ohm 0.8 Low
0 OHm 0.6 Low
Do you have any suggestions as to why this is happening. By the way once the FAULT flag is active and if they slowly increase the impedance going the other way, the FAULT flag is still active all the way until it comes out of over current limit.
Thanks,
Faizul Bacchus