This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS92LV3221: Dual SERDES links in full duplex type setup clock feed through from one chain to the the other

Part Number: DS92LV3221

I am designing a SERDES link with the DS92LV3221/2 devices in a full duplex type configuration with links in either direction between two boards.  The deserializer has an RXCLKOUT which is a reconstructed bit clock from the serializer side.  Can I use this clock to drive another serializer chip?