Could you confirme me that there is not a typo in page 8 (RX_ER/PAUSE_EN).
It specified this pin (46) with PU but in the description of this PIN is the oppossite behaviour:
PAUSE ENABLE: This strapping option allows advertisement of whether or not the DTE(MAC) has implemented both the optional MAC control sublayer and the pause function as specified in clause 31 and annex 31B of the IEEE 802.3x specification (Full Duplex Flow Control).
When left floating the Auto-Negotiation Advertisement Register will be set to 0, indicating that Full Duplex Flow Control is not supported.
When tied low through a 5 kΩ, the Auto-Negotiation Advertisement Register will be set to 1, indicating that Full Duplex Flow Control is supported. The float/pull-down status of this pin is latched into the Auto-Negotiation Advertisement Register during Hardware-Rese