Other Parts Discussed in Thread: SN65HVD233, TCAN330
Hi,
a customer asked me whether the desired part SN65hvd232 would resist a +-30 volt levels transient as well as over a longer period.
These specs are off attention and I need some clarification here:
"voltage at any bus level": is with this level meant, that the device can withstand (without damage) those levels over a certain duration?
the next spec "Voltage input, transient pulse": is this the max transient pulse over which duration that the device can take without damage?
so those questions just for me for clarification.
I already started searching for parts that are higher specified, for example SN65hvd233, which exceeds the +-30 V with the specs mentioned above.
The other device that I found was TCAN330, which also is IEC61000-4-2 specified.
Can I recommend one of those parts in regard of the voltage levels without ESD diode?
Is there another part I have missed, that you can recommend?
Did I understand the specs correctly?
Thank you very much for your help,
best regards,
Marion