Hi Team,
DS90UB913A + DS90UB954-Q1
Imx8mq Android 8.1
It is OK when dispaly test pattern,but in normal prview, the image keeps rolling like below.
Could you give some advices.
Thanks
Chuan
here is the code
ds954_write_reg(ds954_client,0x01,0x02);
msleep(5);
ds954_write_reg(ds954_client,0x33,0x01);
ds954_write_reg(ds954_client,0x4C,0x01);
ds954_write_reg(ds954_client,0x6D,0x7f);
ds954_write_reg(ds954_client,0x20,0x20);
ds954_write_reg(ds954_client,0x1F,0x03);
ds954_write_reg(ds954_client,0x58,0x58);
ds954_write_reg(ds954_client,0x5C,0xB0);
ds954_write_reg(ds954_client,0x5D,0x30);
ds954_write_reg(ds954_client,0x65,0x20);
ds954_write_reg(ds954_client,0x70,0x1E);
ds954_write_reg(ds954_client,0x7C,0xC0);