Part Number: TPS65987D
I am not using the SPI interface on the TPS65987D. It says on the datasheet to ground all the unused SPI pins. Is this correct? This seems like an odd thing to do since this is a SPI master interface and generally the TPS65987D will check if a flash device is connected to it on power up which means it will try driving a signal into a grounded I/O.