Other Parts Discussed in Thread: TIDA-00891
Hi,
- What is the voltage level of the DIR pin? in the data sheet 6.1 Absolute Maximum Ratings it says both VDD5+0.3 & VCC33+0.3. in the sections 8.2.x application diagrams it is pulled high to VCC33 while on the reference design (TIDA-00891 ) it is pulled high to 5V_COM. in the HD3SS3220A-DFP-EVM it is pulled to 3.3V
- What is the DIR polarity? In the data sheet, section 7.2 Functional Block Diagram it shows DIR=0 Tx2/Rx2 as well in the section 7.6.3 Connection Status and Control Register bit 5 description while section 7.3.4 Cable Orientation and Mux Control says : "When a voltage level within the proper threshold is detected on CC1, the DIR pin is pulled low "
Thank you
Doron