Part Number: DP83867IR
Hi Team,
I have a question about EEE with DP83867.
I described comment below so could you help that?
Problem
there is a unit that has EEE function(UNIT 1) and when a board DP838867 is mounted(BOARD 1) is connected to the "UNIT 1" with 10/100M, there is no problem but when "BOARD 1" is connected to the "UNIT 1" with 1000M, "BOARD 1" gets interrupt a lots and transmission is degraded.
when "UNIT 1" EEE is disabled, this interrupt is resolved.
Setting
Disabled: Driver LPI related registers.
Question
From hardware perspective, does DP83867 have any function to address EEE interrupt by register setting?
Thanks,
Kai