This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2034: I need a higher voltage part

Part Number: TPS2034
Other Parts Discussed in Thread: TPS22810

Greetings

I designed a board using this part TPS2034, however I realized too late the part cannot handle a voltage greater than 6Volts.

I need a part that can handle up to 9V, or a discrete design that would work just as well.

Thanks

bkmtech

BKM Engineering

  • Hi, bkmtech,

    The power switch of our product line is USB power switch, so none of power switch of our product line can handle up to 9V. What's your application, isn't it used for USB. If you application is for USB, do you consider to use a DCDC to convert the voltage.

    Anyway, I tried to find this high vin power switch, TPS22810, it's a 18V 3A power switch. Please check if this part meet your requirement. You can also find more parts on www.ti.com.

    Regards,
    Bob