Other Parts Discussed in Thread: SN65HVDA1040A-Q1, SN65HVD1040, TCAN1042-Q1, SN65HVD1040A-Q1
Dear Team,
My customer reported one issue regarding to the SN65HVD1040-Q1.
According to the datasheet 7.1 Absolute Maximum Ratings, it showed that the voltage at bus terminals is limited to the range -27~40V. That means if a bus voltage goes over this voltage limitation, it may cause a permanent damage. Besides, in the 7.3 Recommended Operating Conditions, it showed that the voltage at any bus terminal is limited to the range -12~12V. So my understanding is that when a bus terminal, for example, CANL pin is powered in -12V ~ 12V, it could work normally; if CANL is powered with voltage higher than 12V but lower than the absolute maximum rating voltage, 40V, it may meet the functional failure. this means that it may not work well, but won't have the permanent damage on the device.
Is my understanding correct?
So my customer's observation is as below:
They're doing a reliability test that impose a voltage from a DC voltage source on the CANL pin, GND pin is connected to the source GND. If the voltage is powered with 20V, the SN65HVD1040-Q1 would get permanent damage, After changing a new device, the issue still existed. However, according to the datasheet, if 20V is imposed on the CANL pin, it may not able to work well, but should not get physical damage as it is still within the Absolute Maximum Ratings value. So this behavior is obviously different from what is told on the spec.
Moreover, even with 15V test, the SN65HVD1040-Q1 may still get permanent damage. I'm wondering is this an expected behavior? Or any specific design should be checked carefully?