Part Number: ISO5500
Other Parts Discussed in Thread: UC3845, UC3843
Hello everyone. I am developing a 3kw solar inverter circuit. Currently, I am using ISO5500 to drive IGBT and I have also developed a DC/DC isolated supply using UC3845 with output +15/-8v and .5A for the gate drive supply . The problem is that whenever I connect this dc/dc supply and run my circuit ISO5500 starts producing faults and my system shuts down and when I replace this supply with 15V step-down transformer then I face no such issue the ISO5500 works fine without generating any fault signal. I need help in identifying why ISO5500 is generating a fault signal. Do I need to take any protective measure regarding spurious faults or if the problem is in the Isolated power supply then how to design it correctly for the gate drive application.
Best regards and thanks in advance.