Part Number: TCA6424A
Hi
I have some question about TCA6424A.
#1: If VCCI and VCCP is same voltage, can we use the single power supply source for both VCC rail?
#2: Regarding INT function, I do not understand this function exactly.
Is this a function to notify the CPU side that H / L of input setting port has switched?
If the INT signal is output, can I 2C communicate immediately and check the port?
If it is so, is it possible to use this if control is performed periodically (about 2 ms intervals) to check the port and only the pull-up connection is made without CPU connection?
(Is there any concerns?)
Best Regards,
Koji Hamamoto