This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The main problem at present is that DS90UB925QSQ needs to wait around 5s after receiving imx6 image data to serialize the image data normally (it can be displayed).
Here are the tests and results:
1. Under the condition that the image is normally displayed (it has been waiting for 5s), the PDB pin of 925 is pulled down to enter the power down mode. There is no video output during the period.
2. Under the condition that the image is normally displayed (it has been waiting for 5s), write register 0x01 of 925 and reset it. It is found that it still needs about 5s to restore the normal image output
Help confirm: does it take so long for DS90UB925QSQ to reset each time to send the image data?
sorry for late reply. We find deserializer's data pin can output data soon after serializer start transmission.It not a 925 or 926 issue.Thank you for help!