This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD6S300: TPD6S300

Part Number: TPD6S300

Hi, 

I read the datasheet and it clearly says that all low speed pins are protected against ESD with this chip. What about high speed pins? are these also protected?

Thanks,

Fabio Ruiz 

  • Hi Fabio,
    With TPD6S300 6 channels of IEC 6100-4-2 ESD protection are provided on CC1, CC2, SBU1, SBU2, DP, DM respectively, removing need for high voltage TVS diodes on these lines. With this device ESD protection is not provided on the high speed pins and some external ESD protection device must be included if a customer desires ESD protection on high speed pins.