Part Number: TUSB2046B
Hi,
I have been testing the TUSB2046 with a custom PCB. I am using only 2 downstream devices.
However, the downstream devices do not seem to be detected/connected.
I have attached the USBView screenshots.
Why does the viewer say that the downstream device supports only USB 1.1? Also why is the connection status 'no device connected'?
I have connected the device and I have supplied 5V on the VBUS. The downstream device DP line is high.
I have attached the schematic. 6471.TUSB2046_test.pdf
Please help,
Thanks