This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1002: USB 3.0 camera doesn't work

Part Number: TUSB1002

Hello,

We have a USB 3.0 camera and when we connect it to our custom board it doesn't show any image.We don't have any oscilloscope capable of eye diagram measurement. And the correction with 220k resistors and 330nF were made. |When we connect the device it fallbacks to USB2.0. 

This is the schematic:

System connections: 

Laptop <== USB 3.0 1.8m cable ==> Custom board  with TUSB1002 <== USB 3.0 1.5m cable ==> Camera 

We have an 2GSps oscilloscope available. How would you measure USB 3.0 signal lines to check if the IC is working properly?