This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS25BR120: ICC in case of PE0=1 and PE1

Part Number: DS25BR120

Hi all

Would you mind if we ask DS25BR120?
How much is ICC(supply current) in case of PE0=1 and PE1?
Our customer would like to know maximum current consumption.
There is the description "Figure 13. Power Supply Current as a Function of Frequency".
We assume that this shows typical value.Is it correct?

Typical value in case of PE0=1, PE1=1 : 47mA(from Figure.13)
Maximum value in case of PE0=1, PE1=1 : ??



Kind regards,

Hirotaka Matsumoto