Part Number: DP83822I
Hi,
I have a question about LED pin connections of DP83822I.
I want to setup strap pin LED_0 to MODE 4(AN_0=1)which is default and
LED_0 pin will be connected to LED.
From DP83822 datasheet, resistor RH and RL can be open for setting LED_0 pin to Mode 4.
So, I think the circuit will be like attached file page.1
And also I'm going to connect LED_1 pin to LED as attached file page.1
But I'm not clear that my circuit are correct or not for both cases(LED_0&LED1).
In datasheet page.50 "8.5.2 LED Configuration", it said that parallel resistors are required.
Should I put parallel resistor on LED_0 line and LED_1 line as like attached file page.2 for my use case?
If yes, what value of resistor should be used?
best regards,
g.f.