Hi,
In the datasheet of TCAN1043HG-Q1 it is mentioned that in standby mode INH is high. INH is typically used to Enable 3.3 V power which goes to micro (ref: Application Information section). So if CAN transceiver is in standby mode micro will get powered. CAN transceiver could come to standby mode from internal state or from initial 5 V power up (KL30 on, power chip 5 V on). CAN transceiver can go into standby mode by CAN wakeup from other internal state.My questions are
1.How micro will come to know whether it got powered due CAN wakeup or KL30 on (initial CAN power up)?
2. OEM is asking not to power up micro without CAN wake up. It seems first time CAN transceiver gets power it turns on micro . If this is not acceptable what are the changes that needs be done at circuit level or software level to implement the same?